Skip to main content

If you are looking for a cooling solution to bring you comfort during the summer months, our air conditioners, also known as air-to-air heat pumps, are what you are looking for.

  • Energy efficiency reduces bills and emissions
  • Enjoy comfort at home whatever the weather
  • Improve your indoor air quality
  • Elegant design fits your interior

What are the benefits of an air conditioner or air-to-air heat pump?

Double comfort

Air-to-air heat pumps can provide cooling as well as heating. Enjoy a cool bedroom during summer and a warm living room during winter times.

Cool and heat numerous rooms

A "multi" air-to-air heat pump system lets you link up to five indoor units to one outdoor unit. The indoor units can be of myriad sizes and styles to suit the needs and the design of the space, ensuring you have effective heating and cooling throughout your home. Furthermore, you can vary the temperature in each room. 

Easy to manage

The system is simple to use from anywhere as units are controlled with an easy-to-use remote control or an app.

Cost-effective and sustainable

They also take the worry out of energy bills and environmental impact as they are both cost-effective and sustainable. A mere 20% of the energy needed to run the system comes from electricity. The rest is taken from the ultimate source of renewable energy: the air. So you can rest in the knowledge that your comfort is not costing the earth.

Designed to fit your style

With an extensive range of indoor units, Daikin models are designed to fit in with your style and blend in with your interior giving you optimal comfort throughout the house in any season.

How does an air-to-air heat pump system work?

An air-to-air heat pump comprises two units..

The indoor unit

The air-to-air heat pump indoor unit is the component of the system that’s situated inside the home and supplies the conditioned air into the space. With an extensive range of indoor units, Daikin models are designed to fit in with your style and blend in with your interior giving you optimal comfort throughout the house in any season.

The outdoor unit

The split outdoor unit is the component of an air-to-air heat pump that contains the compressor, propeller fan, circuit board and heat exchanger. It can be mounted on an outside wall or situated on a roof or in a garden. The outdoor unit compresses the refrigerant that takes or releases cold or heat in the room to or from its counterpart indoor unit.

There are three types of air-to-air heat pump indoor units

More information about air conditioning

Yes, and if you renovate your property and switch to renewable air-to-air heat pumps, you will add value to your renovated home, the environment and your pocket. Heat pumps can be installed in almost any home. There are, however some considerations that may need to be addressed, particularly regarding insulation. In order for a heat pump to function at its most efficient, your home needs to be well-insulated to prevent as much heat from escaping as possible. A suitably qualified heating engineer can advise you on what needs to be done in your home in order for it to be appropriate for a heat pump system. This might include upgrading the insulation of your walls and roof. You also need to consider location. The outdoor unit will need to be installed outside your home and should be in a place that you can access easily when you need to clean the unit, adjust its settings or have the heat pump serviced.

Yes, an air-to-air heat pump (also known as an air conditioner) can bring hot water to your home. With Daikin's Multi+ solution, heating, cooling and hot water are supplied with one system. It connects up to three units and one domestic hot water tank and is compatible with a 90 and 120-litre tank and a wide range of indoor units, offering unrivalled flexibility. Our Multi+ solution includes an intuitive full-text display on the domestic hot water tank for monitoring and adjustment of all settings, including scheduling and water temperature.

Daikin's air-to-air heat pumps (also known as air conditioners) can give you relief from your allergies because they can capture the allergens in the heat pump filter and improve the quality of air that you are breathing. Not only do our air-to-air heat pumps keep you warm and cool but they are also removing pollutants, pollen and particle matter from your breathing space.

Some Daikin units are also equipped with a Flash Streamer and different filters like the titanium apatite deodorising filter or the silver allergen removal filter, which are able to reduce the pollutants in the air quickly and efficiently.

No! Furthermore, our air-to-air heat pumps (also known as air conditioners) can help reduce the symptoms of allergies. Daikin integrates multiple filters in all its air conditioning units: titanium deodorising filters, silver allergen filters and flash streamers remove dust and capture bacteria. With proper air conditioning maintenance, and as long as they are cleaned regularly, these filters will provide cleaner, healthier air for everyone to breathe.

 

For your heat pump to function as it should, it is essential that the system is installed correctly. Only an authorised technician should carry out the installation and in a suitable location. The surface must be firm enough to withstand the weight and vibrations of the unit and there must also be sufficient space for airflow and for connecting pipes and power cables. Any plants or shrubs that may be located near your heat pump should be at least a metre away and regularly pruned. The pump should also be installed in a place that’s easy to access for services and other general maintenance.

We often get asked why we can’t put the heat pump inside. Could they not be placed in the loft or conservatory? The answer to this is no. This is because, after a few hours, the heat pump will have extracted all of the warmth from the trapped air, effectively turning this space into a freezer. This is why air-to-air heat pumps need access to the free-flowing outside air.

We advise having a service done by a qualified engineer once a year. Scheduled servicing, regular maintenance spot-checks and routine cleaning of the system will extend its lifespan and maintain its energy efficiency.  

Here are some signs your air-to-air heat pump (also known as air conditioner) needs immediate maintenance:

If your air conditioner unit makes more noise than usual, the filters may be clogged. Clean the unit by removing dust with a vacuum cleaner. If the same noise persists or you hear a gurgling sound, there could be a mechanical issue. A qualified technician should then be called to examine the unit.

Find out which model suits your interior